Re: MPC8640D Failed to reset the target (core did not halt)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re: MPC8640D Failed to reset the target (core did not halt)

933 次查看
badrinath_ngetp
Contributor I

Good Morning,

Please see the attached document.

zip pass 777

Thanks,Regards,

Badri.

+918985740150.

From: nagajyothig@ngetpl.com

Sent: Wed, 08 Jul 2015 05:16:33 +0000

To: discussions-community-about@mail.freescale.jiveon.com

Subject: MPC8640D Failed to reset the target (core did not halt)

 

Hi  all, we are working on a project CPCI Based SBC Board using MPC8640D processor. We are trying to get simple JTAG connection to the processor mpc8640d. We are using code warrior USB tab s/n 0839 0023.  In code warrior, when I try to reset the MPC8640D core (via reset target on launch), it gives the following message:“CCSProtocolPlugin: Failed to reset the target (MPC8640d Core: Core did not halt).”

we are monitoring the jtag signals also , HREST and SRESET signals are not coming..by default these signals are in high state(+3.3v). Can you give me some guidance in interpreting this error ?   Thanks and Regards, Jyothi  

0 项奖励
回复
1 回复

848 次查看
ufedor
NXP Employee
NXP Employee

The "info_11_14.doc" provided in the ZIP contains virus.

0 项奖励
回复