Which clock to use for tDISKEW calculation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which clock to use for tDISKEW calculation

1,654 Views
creinhold
Contributor I

I am investigating an interface between the MPC8308  and a  532MT/s DDR2 RAM and I would like to calculate the the total amount of allowed skew from MDQS to a corresponding MDQ signals tDISKEW.

The document MPC8308 PowerQUICC II Pro, Processor Hardware Specification
Document Number: MPC8308EC, Rev. 4, 12/2014

gives on page 11 a formular to calculate tDISKEW from a clock periode and the controller skew (see attached screenshot). However, it is not mentioned whick clock periode shall be used. Is it the MCK clock periode which in my case would be T=1/133MHz giving a tDISKEW of approx. +/-1ns?

Labels (1)
0 Kudos
Reply
1 Reply

1,542 Views
Bulat
NXP Employee
NXP Employee

You are right, it means MCK clock period. tDISKEW is -1ns (min) to +1ns (max).

Regards,

Bulat

0 Kudos
Reply