We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

1,123件の閲覧回数
kamalakannanr
Contributor I

We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

0 件の賞賛
返信
1 返信

984件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Attached our Networking Product Selector guide.

Please look devices:

T1040/T1042 - "Value-performance" segment

T2080/T2081 - mid-performance segment

T4240 - High-performance segment

0 件の賞賛
返信