We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

1,762 次查看
kamalakannanr
Contributor I

We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

0 项奖励
回复
1 回复

1,623 次查看
alexander_yakov
NXP Employee
NXP Employee

Attached our Networking Product Selector guide.

Please look devices:

T1040/T1042 - "Value-performance" segment

T2080/T2081 - mid-performance segment

T4240 - High-performance segment

0 项奖励
回复