U-Boot for PowerQUICC Based Designs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-Boot for PowerQUICC Based Designs

1,290 Views
stacym
Contributor I

I have found the app note (AN4173) that addresses customization of U-Boot for the i.MX51.  Is there a similar app note for the MPC8308 or the Power QUICC family of devices?  I am looking for some help in modifying U-Boot for some customized hardware.

Thanks!

Tags (1)
0 Kudos
Reply
1 Reply

1,104 Views
lunminliang
NXP Employee
NXP Employee

I am not aware of that kind of document, there are two FTF presentation with the document number "FTF12-NET-F0180" and "FTF11-NET-F0399", they are talking about QorIQ P5 Processor, "Overcome the Challenges in Porting U-Boot and Linux OS", maybe your can refer to. The two presentation could be download from www.freescale.com.

0 Kudos
Reply