U-Boot for PowerQUICC Based Designs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

U-Boot for PowerQUICC Based Designs

1,313 次查看
stacym
Contributor I

I have found the app note (AN4173) that addresses customization of U-Boot for the i.MX51.  Is there a similar app note for the MPC8308 or the Power QUICC family of devices?  I am looking for some help in modifying U-Boot for some customized hardware.

Thanks!

标记 (1)
0 项奖励
回复
1 回复

1,127 次查看
lunminliang
NXP Employee
NXP Employee

I am not aware of that kind of document, there are two FTF presentation with the document number "FTF12-NET-F0180" and "FTF11-NET-F0399", they are talking about QorIQ P5 Processor, "Overcome the Challenges in Porting U-Boot and Linux OS", maybe your can refer to. The two presentation could be download from www.freescale.com.

0 项奖励
回复