T4240 Memory problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4240 Memory problems

1,906件の閲覧回数
jack_huang1
Contributor IV

T4240rm states that each channel has a maximum of 64GB, but it is later explained that each slice supports a maximum of 4GB, which is inconsistent? How much memory capacity can this chip support? What are the restrictions on chip selection or memory chip
Because we tested the 16GB UDImm memory strip on the development board QDS, some of the memory was not available, and some of the RDImm was available. The maximum was only 16GB.

Thank you.

ラベル(1)
  • DDR

タグ(1)
0 件の賞賛
返信
1 返信

1,863件の閲覧回数
ufedor
NXP Employee
NXP Employee

QorIQ T4240 Reference Manual, 11.5 DDR Functional Description:

"Bank sizes up to 16 Gbytes are supported, providing up to a maximum of 64 Gbytes of DDR main memory."

0 件の賞賛
返信