Supported codewarrior IDE version for the MPC860

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Supported codewarrior IDE version for the MPC860

2,285件の閲覧回数
maheshwarreddy
Contributor I

Now we are using the MPC860 power Quicc processor . we had installed the codewarrior 10.5.1 but we are unable to find the MPC860 series device .which version of the codewarrior we need to install . 

タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,170件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use CodeWarrior 8.8 classic edition for the MPC860. See attached snapshots.

 

This CodeWarrior is available using the following link:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-ARCHT-EX

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,170件の閲覧回数
maheshwarreddy
Contributor I

Thank you for the reply .

I had installed the code warrior v8.8 while installing the code warrior we are getting the error as cannot run an x86 buit of this utility on x64 platform .How to solve this issue.

Thank you 

Best regards

Maheshwar

0 件の賞賛
返信