Supported codewarrior IDE version for the MPC860

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Supported codewarrior IDE version for the MPC860

2,478 Views
maheshwarreddy
Contributor I

Now we are using the MPC860 power Quicc processor . we had installed the codewarrior 10.5.1 but we are unable to find the MPC860 series device .which version of the codewarrior we need to install . 

Tags (3)
0 Kudos
Reply
2 Replies

2,363 Views
Pavel
NXP Employee
NXP Employee

Use CodeWarrior 8.8 classic edition for the MPC860. See attached snapshots.

 

This CodeWarrior is available using the following link:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-ARCHT-EX

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,363 Views
maheshwarreddy
Contributor I

Thank you for the reply .

I had installed the code warrior v8.8 while installing the code warrior we are getting the error as cannot run an x86 buit of this utility on x64 platform .How to solve this issue.

Thank you 

Best regards

Maheshwar

0 Kudos
Reply