Supported code warrior version for the TWR MPC5125

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Supported code warrior version for the TWR MPC5125

1,933件の閲覧回数
maheshwarreddy
Contributor I

Hai,

We want to use the TWR MPC5125 tower module , Which version of the code warrior is compatible can you please suggest us .

Thank you

Best regards

Maheshwar.

ラベル(1)
  • DDR

0 件の賞賛
返信
2 返答(返信)

1,756件の閲覧回数
maheshwarreddy
Contributor I

Hai ,Pavel Chubakov 

Thank you for the reply . i installed the code warrior mobile gt 9.2 but while installing its giving the error .I continued but after opening the IDE if i create a project when i compiled that time it is error as below.

error unable to call the command line tool. check your path environmental variable.

find the below attachment.Screenshot (16).png

0 件の賞賛
返信

1,756件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use NXP CodeWarrior MGT 9.2 for the TWR-MPC5125:

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/mpc5xxx-5...

 

This CodeWarrior supports CodeWarrior TAP and can be used under Windows 7, Windows 8 and Windows 10.

There is also Linux version of this CodeWarrior.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信