Segger J-Link with LS1046A Freeway

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Segger J-Link with LS1046A Freeway

跳至解决方案
3,117 次查看
jekim
Contributor IV

Hello,

I installed CodeWarrior Studio 11.5.2. I'm trying to add new connection for LS1046A Freeway. It seems the probe type is fixed to CWTAP. Is it possible to add segger J-Link in the connection? Thanks.

Best Regards,

Jeff

标记 (3)
0 项奖励
回复
1 解答
3,113 次查看
ufedor
NXP Employee
NXP Employee

You wrote:

> Is it possible to add segger J-Link in the connection?

This is not possible.

在原帖中查看解决方案

3 回复数
3,114 次查看
ufedor
NXP Employee
NXP Employee

You wrote:

> Is it possible to add segger J-Link in the connection?

This is not possible.

3,103 次查看
jekim
Contributor IV

Dear Fedor,

 

Thank you for the confirmation. Then, below base unit and tip are enough for LS1046A Freeway debug?

CWH-CTP-CTX10-YE Product Information|NXP

CWH-CTP-BASE-HE Product Information|NXP

 

Best Regards,

Jeff

0 项奖励
回复
3,096 次查看
ufedor
NXP Employee
NXP Employee

Yes, these are correct TAP and Probe Tip for ARM processors.

0 项奖励
回复