Reset sequence is not working in T1014NXEPQA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reset sequence is not working in T1014NXEPQA

1,020件の閲覧回数
EC146552
Contributor I

Asleep signal is always coming low while starting of reset sequence of T1014NXWPQA.

First, we are providing POR and then T1014 is driving HRST signal low but when POR is high then after 3ms HRST_REQ signal is coming from processor and then againg we are providing POR low and this sequence is repeating again and again.

and  throughout this ASLEEP is low.

how to generate reset sequence for T1014?

please help

0 件の賞賛
返信
1 返信

896件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section# 4.7.1 and figure# 4-1 of the T1024RM and let me know from which part of the sequence is the system going wrong.

 

Also, share the complete debug logs and if possible the schematic of the design.

0 件の賞賛
返信