Reprogramming DDR controller on PowerQUICC III

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reprogramming DDR controller on PowerQUICC III

1,406件の閲覧回数
ConfusedInOR
Contributor I

Is it possible to reprogram the DDR controller on PowerQUICC III more than once after power-up?  Our system uses two bootROM (once factory installed, one field-upgradable) and the DDR is programmed in both (not necessarily with the same settings).  Is there a different program sequence needed the second time though?  Thanks!

0 件の賞賛
返信
0 返答(返信)