Reprogramming DDR controller on PowerQUICC III

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reprogramming DDR controller on PowerQUICC III

1,414 Views
ConfusedInOR
Contributor I

Is it possible to reprogram the DDR controller on PowerQUICC III more than once after power-up?  Our system uses two bootROM (once factory installed, one field-upgradable) and the DDR is programmed in both (not necessarily with the same settings).  Is there a different program sequence needed the second time though?  Thanks!

0 Kudos
Reply
0 Replies