QE Microcode download problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QE Microcode download problem

ソリューションへジャンプ
4,690件の閲覧回数
00lirui
Contributor I

     I made a board according to MPC8306SOM , and download the uboot.bin. The QE can't work and hangs at "Net:". I found the problem is caused by the lack of QE ROM ,so I must download the qe firmware to flash , However I can't find the proper version of mpc8306 qe from websit "http://opensource.freescale.com/firmware/",and don't know which address of flash to be download,The address was defined in the mpc8306som.h ,"#define CONFIG_SYS_QE_FW_ADDR   0xFE7E0000" . Should I download firmware at  0xfff00000 address?  the start address of flash is 0xff800000.

    thanks!

0 件の賞賛
返信
1 解決策
4,296件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, uboot binary image does not contain microcode image, microcode image should be programmed to specified location in flash, as described in the document I mentioned above.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,296件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please let me know which Linux BSP you are using. In case if you are using Linux BSP from MPC8306SOM board, than this procedure of QE microcode upload is implemented already in this BSP, and QE microcode image is distributed as a part of this BSP.

0 件の賞賛
返信
4,296件の閲覧回数
00lirui
Contributor I

Hi

  I install the mpc8306 ltib and build the uboot image, download and try ,the output printf message is " Not a microcode" and hangs at "Net:".

So ,the problem remains.

  thank you !

0 件の賞賛
返信
4,296件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Uboot image definitely does not contain QE microcode image, it is a separate file. What do you think about reading documentation included in Linux BSP?

\help\software\tools_8309som\nor_flashing\ NOR Flash Programming User Manual.pdf

4,296件の閲覧回数
00lirui
Contributor I

       Are you sure that uboot don't contain microcode image? If so ,How to find the separate file ,and how to make it work?

0 件の賞賛
返信
4,297件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, uboot binary image does not contain microcode image, microcode image should be programmed to specified location in flash, as described in the document I mentioned above.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,296件の閲覧回数
00lirui
Contributor I

     I installed the ltib-mpc8308erdb,and used it to compile the u-boot-2009.11 for mpc8306. I read the QE manual and find mpc8308 don't have QE. So,Do I neet to install mpc8309 ltib instead?

0 件の賞賛
返信