Packet loss with MPC8347 DR UDC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Packet loss with MPC8347 DR UDC

3,810 Views
cpark
Contributor II

Hi,

I have a data corruption (or packet loss) problem with MPC8347 USB Device Controller.

I am using our 8347 custom board as USB Device and a laptop as USB Host.

My test application sends data from USB Device to USB Host.

       MPC8347 (Device) -----> Laptop (Host)

It sends 1448 bytes of data to the host in the following structure.

unsigned int buf[362];

buf[0] = 1;    // sequence number

buf[1] = 1440; // data length in byte

buf[2] = 0xDEADBEEF;

buf[3] = 0xDEADBEEF;

buf[361] = 0xDEADBEEF;

There is 2 ms delay after the write and it sends another 1448 bytes of data in the same structure with sequence number incremented by 1.

The device keeps sending data and the host receives and verifies the data.

It works quiet well for about 10~20 minutes and the problem occurs.

The problem is that the host expects to receive 0xDEADBEEF, but it receives wrong data.  In fact, it receives the sequence number of the next data packet.

It looks like there is packet loss in DR (Dual-Role) UDC.

Would this be a known issue with DR UDC?  Could you confirm that it is caused by USB-A001 in MPC8349E Chip Errata?

The MPC8347 board is running Linux 3.2.   My laptop is running Ubuntu 12.04.

Here is configuration of DR UDC in my kernel.

  usb@23000 {

     compatible = "fsl-usb2-dr";

     reg = <0x23000 0x1000>; // OK, USB DR starts at 0x23000

     #address-cells = <1>;

     #size-cells = <0>;

     interrupt-parent = <&ipic>;

     interrupts = <38 0x8>; // OK, IRQ ID no = 38 for USB-DR

     dr_mode = "peripheral";

     phy_type = "ulpi";

  };

Here is output of lsusb -v on my laptop.  It shows information of MPC8347 Gadget driver.

Bus 001 Device 110: ID xxxx:yyyy ABCD

Device Descriptor:

  bLength                18

  bDescriptorType         1

  bcdUSB               2.00

  bDeviceClass            0 (Defined at Interface level)

  bDeviceSubClass         0

  bDeviceProtocol         0

  bMaxPacketSize0        64

  idVendor           0xxxxx ABCD

  idProduct          0xyyyy

  bcdDevice            2.19

  iManufacturer           1 ABCD

  iProduct                2 ABCD

  iSerial                 3 ABCDABCD

  bNumConfigurations      1

  Configuration Descriptor:

    bLength                 9

    bDescriptorType         2

    wTotalLength           32

    bNumInterfaces          1

    bConfigurationValue     1

    iConfiguration          0

    bmAttributes         0xc0

      Self Powered

    MaxPower                2mA

    Interface Descriptor:

      bLength                 9

      bDescriptorType         4

      bInterfaceNumber        0

      bAlternateSetting       0

      bNumEndpoints           2

      bInterfaceClass         7 Printer

      bInterfaceSubClass      1 Printer

      bInterfaceProtocol      2 Bidirectional

      iInterface              0

      Endpoint Descriptor:

        bLength                 7

        bDescriptorType         5

        bEndpointAddress     0x81  EP 1 IN

        bmAttributes            2

          Transfer Type            Bulk

          Synch Type               None

          Usage Type               Data

        wMaxPacketSize     0x0200  1x 512 bytes

        bInterval               0

      Endpoint Descriptor:

        bLength                 7

        bDescriptorType         5

        bEndpointAddress     0x01  EP 1 OUT

        bmAttributes            2

          Transfer Type            Bulk

          Synch Type               None

          Usage Type               Data

        wMaxPacketSize     0x0200  1x 512 bytes

        bInterval               0

Device Qualifier (for other device speed):

  bLength                10

  bDescriptorType         6

  bcdUSB               2.00

  bDeviceClass            7 Printer

  bDeviceSubClass         0

  bDeviceProtocol         0

  bMaxPacketSize0        64

  bNumConfigurations      1

Device Status:     0x0001

  Self Powered

Best regards,

Chan

0 Kudos
Reply
9 Replies

3,172 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Park,

Please check whether the following errata would be helpful for you.

USB31: Transmit data loss based on bus latency

Description: Devices: MPC8349E, MPC8347E, MPC8343E

When acting as a Device, after receiving a Token IN, the USB controller will reply with a data

packet. If the bus memory access is not fast enough to backfill the TX fifo, it will cause an

under-run. In this situation a CRC error will be introduced in the packet and the Host will ignore

it. However, when an underrun happens, the TX fifo will get a flush command. This situation

may cause an inconsistence in the TX fifo controls, leading to a possible data loss (a complete

packet or sections of a packet can be never transmitted). This situation may also happen if the

software issues a TX flush command.

Impact: When the USB controller is configured as a device, it can not be used in the stream mode due

to this erratum. Therefore, the USB external bus utilization is decreased.

Workaround: A valid software workaround is to disable the stream mode by setting USBMODE[SDIS] bit.

This can avoid the issue at the expense of decreased USB external bus utilization.

Fix plan: No plans to fix

M


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,172 Views
cpark
Contributor II

Hi Yiping,

Thanks for sharing the information.

Actually, I have already tested STREAM_DISABLE and found that the problem still occurs even with Stream Mode disabled.

Here is code changes I have applied to the FSL UDC core driver (Linux 3.2) to disable Steam Mode.

diff --git a/drivers/usb/gadget/fsl_udc_core.c b/drivers/usb/gadget/fsl_udc_core.c

index 01de16e..1a3e3d3 100644

--- a/drivers/usb/gadget/fsl_udc_core.c

+++ b/drivers/usb/gadget/fsl_udc_core.c

@@ -295,6 +295,7 @@ static int dr_controller_setup(struct fsl_udc *udc)

        tmp = fsl_readl(&dr_regs->usbmode);

        tmp &= ~USB_MODE_CTRL_MODE_MASK;        /* clear mode bits */

        tmp |= USB_MODE_CTRL_MODE_DEVICE;

+       tmp |= USB_MODE_STREAM_DISABLE;

        /* Disable Setup Lockout */

        tmp |= USB_MODE_SETUP_LOCK_OFF;

        if (udc->pdata->es)

@@ -363,6 +364,7 @@ static void dr_controller_run(struct fsl_udc *udc)

        /* Set the controller as device mode */

        temp = fsl_readl(&dr_regs->usbmode);

        temp |= USB_MODE_CTRL_MODE_DEVICE;

+       temp |= USB_MODE_STREAM_DISABLE;

        fsl_writel(temp, &dr_regs->usbmode);

        /* Set controller to Run */

Apparently, this problem seems to happen due to USB-A001.  I think so because if I remove the 2ms delay between 1448 Bytes transfers, the problem disappears for more than 15 hours.

Having the delay between transfers, the problem appears after 10 minutes to 5 hours of testing (I would say, it happens randomly).

I really appreciate if you can shed some light on this urgent issue as this problem is quiet ciritical to our product.

USB-A001: Last read of the current dTD done after USB interrupt

Description: Devices: MPC8349E, MPC8347E, MPC8343E

After executing a dTD, the device controller executes a final read of the dTD terminate bit. This

is done in order to verify if another dTD has been added to the linked list by software right at

the last moment.

It was found that the last read of the current dTD is being performed after the interrupt was

issued. This causes a potential race condition between this final dTD read and the interrupt

handling routine servicing the interrupt on complete which may result in the software freeing

the data structure memory location, prior to the last dTD read being completed. This issue is

only applied to a USB device controller.

Best regards,

Chan

0 Kudos
Reply

3,172 Views
lunminliang
NXP Employee
NXP Employee

How do you build your system? Is your USB device a storage device or printer?

0 Kudos
Reply

3,172 Views
cpark
Contributor II

Hi lunminliang,

It is a printer device.

drivers/usb/gadget/printer.c

Thanks,

Chan

0 Kudos
Reply

3,172 Views
lunminliang
NXP Employee
NXP Employee

1. Can you use a USB protocol analyzer to check whether the data have been sent out from the USB PHY of the 834x  to the USB host?

2. I would like to check the data package send out from the USB controller on the ULPI interface to isolate the problem if the missing data is confirmed from the step 1.

0 Kudos
Reply

3,172 Views
cpark
Contributor II

Hi lunminliang,


Based on the following description, I have added 10us delay in the interrupt handling routine (tx_complete()) and it appears that the problem goes away.  Do you think it can be a valid workaround?   If yes, would the 10us delay be enough?  

USB-A001: Last read of the current dTD done after USB interrupt

Description: Devices: MPC8349E, MPC8347E, MPC8343E

After executing a dTD, the device controller executes a final read of the dTD terminate bit. This

is done in order to verify if another dTD has been added to the linked list by software right at

the last moment.

It was found that the last read of the current dTD is being performed after the interrupt was

issued. This causes a potential race condition between this final dTD read and the interrupt

handling routine servicing the interrupt on complete which may result in the software freeing

the data structure memory location, prior to the last dTD read being completed. This issue is

only applied to a USB device controller.

Thanks

Chan Park

0 Kudos
Reply

3,172 Views
lunminliang
NXP Employee
NXP Employee

See apps comment:

If it works, it could be a solution for your system. If it is really the USB-A001 issue, 10 us delay should be enough. I assume that the platform clock is > 100 MHz.

0 Kudos
Reply

3,172 Views
cpark
Contributor II

The following change solved the issue with USB-A001.

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/?h=imx_2.6.35_maintain&id=f34bd00...

As far as I know, this is a common problem with Chipidea IP.  Newer Chipidea IP would not have such issue though.

I am glad there is a workaround for this problem. :smileyhappy:

0 Kudos
Reply

3,172 Views
cpark
Contributor II

I managed to reproduce the problem again and recorded the traffic using Ellisys USB Analyzer.

Here is the screen shot showing the packet loss problem.

MPC8347 DR UDC Packet Loss.png

0 Kudos
Reply