P1022 SDRAM test failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1022 SDRAM test failed

1,455 Views
sarkarsouvik
Contributor II

Hello All,

We are testing a custom board with processor P1022. The processor boots but is always stuck on the SDRAM test phases. This is observed in 2 of 15 boards so we do not consider it the problem of routing. 

The power supplies, clocks to the DDR, and reset are checked and found to be ok.

Please help regarding this issue.

Thanks and Regards,

Souvik

Labels (1)
0 Kudos
Reply
1 Reply

1,444 Views
yipingwang
NXP TechSupport
NXP TechSupport

You could use QCVS DDRv tool to connect to your custom board to do optimization and validation.

You could use CodeWarrior to connect to your custom board to read DDR configuration register values, then modify the attached file according to these register values. Then create a QCVS DDR project with "Import from memory file" method, using the modified file.

0 Kudos
Reply