hi experts
I am afraid I can't express what I think in English well. But I hope you can understand it
i used U-boot and kernel from QorIQ-SDK-V1.8
when i used P1011-FCM with HW_ECC_MODE + UBI filesystem
there is no error
recently in some of our products there is a ecc error in U-boot ( when i nanddump the region which reported ecc erros, there are 1 or 2 bits errors)
so i tried to set FCM to disable ECC and try to use NAND_ECC_SOFT_BCH
in kernel and U-boot i changed ecc.mode ( below is what is chaged)
in dirver/mtd/nand/fsl_elbc_nand.c
static int fsl_elbc_chip_init(struct fsl_elbc_mtd *priv)
- chip->ecc.mode = NAND_ECC_SOFT
+ chip->ecc.mode = NAND_ECC_SOFT_BCH
in U-boot there is no error
but in Kernel when i access nand space , i got erros about ECC
root@p1020rdb-pd:~# flash_erase /dev/mtd3 0 0
Erasing 128 Kibyte @ 13e0000 -- 100 % complete
root@p1020rdb-pd:~# ubiformat /dev/mtd3
ubiformat: mtd3 (nand), size 20971520 bytes (20.0 MiB), 160 eraseblocks of 131072 bytes (128.0 KiB), min. I/O size 2048 bytes
libscan: scanning eraseblock 159 -- 100 % complete
ubiformat: 160 eraseblocks are supposedly empty
ubiformat: formatting eraseblock 159 -- 100 % complete
root@p1020rdb-pd:~# ubiattach -m 3
[ 511.034744] UBI: attaching mtd3 to ubi0
[ 511.041059] ecc unrecoverable error
[ 511.044593] UBI warning: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB 2:0, read only 64 bytes, retry
[ 511.056915] ecc unrecoverable error
[ 511.060452] UBI warning: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB 2:0, read only 64 bytes, retry
[ 511.072135] ecc unrecoverable error
[ 511.075728] UBI warning: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB 2:0, read only 64 bytes, retry
[ 511.088458] ecc unrecoverable error
[ 511.091997] UBI error: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB 2:0, read 64 bytes
[ 511.101833] CPU: 0 PID: 1908 Comm: ubiattach Not tainted 3.12.37-rt51-QorIQ-SDK-V1.8+gf488de6 #50
[ 511.110710] Call Trace:
[ 511.113173] [df061ce0] [c0006c7c] show_stack+0x44/0x16c (unreliab
any tips and ideas are appreciated
thanks in advance
Solved! Go to Solution.
In file include/configs/p1_p2_rdb_pc.h in u-boot, please modify the source code as the following.
#define CONFIG_SYS_NAND_BR_PRELIM (BR_PHYS_ADDR(CONFIG_SYS_NAND_BASE_PHYS) \
| (2<<BR_DECC_SHIFT) /* Use HW ECC */ \
| BR_PS_8 /* Port Size = 8 bit */ \
| BR_MS_FCM /* MSEL = FCM */ \
| BR_V) /* valid
=>
#define CONFIG_SYS_NAND_BR_PRELIM (BR_PHYS_ADDR(CONFIG_SYS_NAND_BASE_PHYS) \
| BR_DECC_OFF /* no error corr */ \
| BR_PS_8 /* Port Size = 8 bit */ \
| BR_MS_FCM /* MSEL = FCM */ \
| BR_V) /* valid
In Linux Kernel, please enable MTD_NAND_ECC_BCH.
Symbol: MTD_NAND_ECC_BCH [=n] 
Type : boolean 
Prompt: Support software BCH ECC
     Location:
         -> Device Drivers
             -> Memory Technology Device (MTD) support (MTD [=y]) 
                 -> NAND Device Support (MTD_NAND [=y])
i did it in u-boot ..so i can read kenrel and rootfilesystem without error from nand
in kernel , JFFS2 filesystem works without error
i think ubi or jffs2 file system use mtd layer , and mtd layer use nand read and write function
if nand read and write funciton has problems jffs2 access shoudn't work
am i wrong ?
In file include/configs/p1_p2_rdb_pc.h in u-boot, please modify the source code as the following.
#define CONFIG_SYS_NAND_BR_PRELIM (BR_PHYS_ADDR(CONFIG_SYS_NAND_BASE_PHYS) \
| (2<<BR_DECC_SHIFT) /* Use HW ECC */ \
| BR_PS_8 /* Port Size = 8 bit */ \
| BR_MS_FCM /* MSEL = FCM */ \
| BR_V) /* valid
=>
#define CONFIG_SYS_NAND_BR_PRELIM (BR_PHYS_ADDR(CONFIG_SYS_NAND_BASE_PHYS) \
| BR_DECC_OFF /* no error corr */ \
| BR_PS_8 /* Port Size = 8 bit */ \
| BR_MS_FCM /* MSEL = FCM */ \
| BR_V) /* valid
In Linux Kernel, please enable MTD_NAND_ECC_BCH.
Symbol: MTD_NAND_ECC_BCH [=n] 
Type : boolean 
Prompt: Support software BCH ECC
     Location:
         -> Device Drivers
             -> Memory Technology Device (MTD) support (MTD [=y]) 
                 -> NAND Device Support (MTD_NAND [=y])
thanks