NAND bitflip correction on 8314

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NAND bitflip correction on 8314

跳至解决方案
2,412 次查看
jefftharris
Contributor I

Does the NAND controller on the 8314 CPU provide notification for an ECC-corrected bitflip error?  The 8313 CPU contains the LTECCR register.  Does the 8314 support this register as well?  If not, is there another method to detect the condition so the Linux UBI driver can scrub the block before an unrecoverable error occurs?

1 解答
2,145 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes there are MPC83xx eLBC which do not have LTECCR register. According to MPC8314 documentation there is not LTECCR. The Freescale Enhanced Local Bus Controller NAND driver (fsl_elbc_nand.c) says that "if the ELBC doesn't have the lteccr register it reads 0".So it read it always

if (lteccr & 0x000F0000) {
       mtd->ecc_stats.corrected++;
       elbc_fcm_ctrl->max_bitflips = 1;
 

but without LTECCR ecc_stats.corrected will be not incremented. I do not see another method with hardware support in this case. Of course there is bulky method when we read the same page two times first when ECC correction is enabled and second when it is disabled and then compare.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,146 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes there are MPC83xx eLBC which do not have LTECCR register. According to MPC8314 documentation there is not LTECCR. The Freescale Enhanced Local Bus Controller NAND driver (fsl_elbc_nand.c) says that "if the ELBC doesn't have the lteccr register it reads 0".So it read it always

if (lteccr & 0x000F0000) {
       mtd->ecc_stats.corrected++;
       elbc_fcm_ctrl->max_bitflips = 1;
 

but without LTECCR ecc_stats.corrected will be not incremented. I do not see another method with hardware support in this case. Of course there is bulky method when we read the same page two times first when ECC correction is enabled and second when it is disabled and then compare.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,145 次查看
jefftharris
Contributor I

NXP confirmed the 8314 does not have the register.  The double-read method works but is slow as expected.

Jeff

0 项奖励
回复