8308 hwconfig word

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

8308 hwconfig word

1,048 次查看
hyoungkikim
Contributor IV

hello experts

my board use a flash  for hw reset configration word  ( CFG_RESET_SORUCE is  NOR FLASH)

i changed hw reset configration word to change core clock

but after re-program a flash   a  board won't boot

and hard reset  signal from 8308  is asserted   ( never de-asserted)   so i can't use codewarriror usb tap to re-program a flash

i checked CS0 and address line  singals  and they are  working  ( i think  mpc8308 tries to get valid hw reset configration word)

if hw reset configration is wrong     can mpc8308   assert hard reset signal ?

than  how can i re-program a flash ?

thanks you

标记 (1)
0 项奖励
回复
2 回复数

920 次查看
alexander_yakov
NXP Employee
NXP Employee

Please press Edit - Preferences - Remote Connections, select your debug probe in the list, click "Change", new window with debug probe settings will appear, in this window please enable "Use JTAG Configuration File" checkbox and "Choose" button below. Here please select and pick one of MPC8308* files from the following folder:

[your CodeWarrior path]\PowerPC_EABI_Support\Initialization_Files\jtag_chains\


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

920 次查看
sinanakman
Senior Contributor III

Hi Hyoung

Most JTAG debuggers would provide a mechanism

to override RCW. I am not sure about CodeWarriror

you are using but I have a BDI3000 (from Abatron)

and with it, it would possible to define a new RCW in

the config file to override the one from flash and boot

the board properly.

Hope this helps

Regards

Sinan Akman

0 项奖励
回复