We do not offer ready to use document for migration from MPC8270 to MPC8271, unfortunately.
Please look application note AN2291, this document describes differences among MPC82xx family devices.
Generally yes, MPC8280 and MPC8272 families are very similar, and software created for MPC8280 will work with no (or very minor) modifications on MPC8272.
The only major difference is MCC - MPC8272 family does not have MCC controller, it has "QMC" controller instead.
If this functionality is not used in your design, than all other functions may be easily migrated.
Note, MPC8272 is "reduced" version of MPC8280 - it has less number of SCCs and FCCs, less amount of internal DPRAM memory, but yes - available in 400 Mhz core version for 516-pin PBGA package.
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------