MPC8640D JTAG problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8640D JTAG problem

1,946 Views
jeffcao
Contributor I

I am facing issue while connecting JTAG with MPC8640 board.I am using WINDRIVER debug 8640D.

in the process "attemping JTAG communication " it display fail.

what might be the problem?

I found it can distinguish two core。

but it cannt be conmmunicate with the  2 core 

0 Kudos
Reply
3 Replies

1,817 Views
alexander_yakov
NXP Employee
NXP Employee

Debug interface is a part of core, so if the core is disabled, debug interface is also inaccessible.

This is the most frequent reason for the core to not respond to debugger commands.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,817 Views
jeffcao
Contributor I

you say ”This is the most frequent reason for the core to not respond to debugger command”

How can I prove this viewpoint.

power on sequence I have been check 

No abnormality found

0 Kudos
Reply

1,817 Views
alexander_yakov
NXP Employee
NXP Employee

In addition to power supply, there are a lot of other things to check:

1. Reset configuration

2. Clock frequency and clock settings

3. etc

0 Kudos
Reply