MPC8548 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8548 processor

1,460件の閲覧回数
lakshmit
Contributor I

can MPC8548 processor write data from PCIe interface to DDR2 without affecting the core operation?

0 件の賞賛
返信
1 返信

1,376件の閲覧回数
ufedor
NXP Employee
NXP Employee

Yes, the MPC8548 DMA controller could be used to write data from the PCI Express interface outbound ATMU to DDR2 without affecting the core operation.


Best regards,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信