MPC8548 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8548 processor

1,496 Views
lakshmit
Contributor I

can MPC8548 processor write data from PCIe interface to DDR2 without affecting the core operation?

0 Kudos
Reply
1 Reply

1,412 Views
ufedor
NXP Employee
NXP Employee

Yes, the MPC8548 DMA controller could be used to write data from the PCI Express interface outbound ATMU to DDR2 without affecting the core operation.


Best regards,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply