MPC8544 Speed grades

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8544 Speed grades

Jump to solution
2,634 Views
edmoore
Contributor I

We are currently using a MPC8544VJAQGA in a product. That's running with a 400M platform clock and 1000M core clock.  Can we use a MPC8544VJARJA (spec'd at 533M platform, 1067M core) at our exisitng clock rates, without any problem ? In other words, is the faster part guaranteed to run at the slower rate ? 

--ed

0 Kudos
Reply
1 Solution
2,620 Views
r8070z
NXP Employee
NXP Employee

Yes you can use a MPC8544VJARJA (spec'd at 533M platform, 1067M core) at our existing clock rates (suitable for MPC8544VJAQGA ), without any problem.

View solution in original post

0 Kudos
Reply
1 Reply
2,621 Views
r8070z
NXP Employee
NXP Employee

Yes you can use a MPC8544VJARJA (spec'd at 533M platform, 1067M core) at our existing clock rates (suitable for MPC8544VJAQGA ), without any problem.

0 Kudos
Reply