MPC8544 Speed grades

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,628件の閲覧回数
edmoore
Contributor I

We are currently using a MPC8544VJAQGA in a product. That's running with a 400M platform clock and 1000M core clock.  Can we use a MPC8544VJARJA (spec'd at 533M platform, 1067M core) at our exisitng clock rates, without any problem ? In other words, is the faster part guaranteed to run at the slower rate ? 

--ed

0 件の賞賛
返信
1 解決策
2,614件の閲覧回数
r8070z
NXP Employee
NXP Employee

Yes you can use a MPC8544VJARJA (spec'd at 533M platform, 1067M core) at our existing clock rates (suitable for MPC8544VJAQGA ), without any problem.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,615件の閲覧回数
r8070z
NXP Employee
NXP Employee

Yes you can use a MPC8544VJARJA (spec'd at 533M platform, 1067M core) at our existing clock rates (suitable for MPC8544VJAQGA ), without any problem.

0 件の賞賛
返信