MPC8533EVJANGA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,021件の閲覧回数
meo081101
Contributor II

Hello,

Can I replace a MPC8533VTALF by a MPC8533EVJANGA?

Can you give me document that shows diffirent between MPC8533VTALF and MPC8533EVJANGA?

Thank you!

Kean

1 解決策
1,937件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Please see section 22.2 “Nomenclature of Parts Fully Addressed by this Document” in the data sheet

https://www.nxp.com/docs/en/data-sheet/MPC8533EEC.pdf

Using table Table Device Nomenclature you can easily see the differences. Notice for migration from VT device to VJ device there is PCN “Device Migration from Leaded Wafer Bumps to Lead-Free Wafer Bumps”

https://www.nxp.com/docs/en/product-change-notice/PCN16365.htm

For each MPC8533 device you can get details on the nxp site. For example for the MPC8533EVJANGA see page

https://www.nxp.com/part/MPC8533EVJANGA

Because these devices have different revision  you may need to check the MPC8533 errata, some issues have been fixed on new revision. Unfortunately it is not public document (requires for NDA).

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,938件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Please see section 22.2 “Nomenclature of Parts Fully Addressed by this Document” in the data sheet

https://www.nxp.com/docs/en/data-sheet/MPC8533EEC.pdf

Using table Table Device Nomenclature you can easily see the differences. Notice for migration from VT device to VJ device there is PCN “Device Migration from Leaded Wafer Bumps to Lead-Free Wafer Bumps”

https://www.nxp.com/docs/en/product-change-notice/PCN16365.htm

For each MPC8533 device you can get details on the nxp site. For example for the MPC8533EVJANGA see page

https://www.nxp.com/part/MPC8533EVJANGA

Because these devices have different revision  you may need to check the MPC8533 errata, some issues have been fixed on new revision. Unfortunately it is not public document (requires for NDA).

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,937件の閲覧回数
meo081101
Contributor II

Have a nice day,

Thank you for your helpful answer!

0 件の賞賛
返信