MPC8349 TSEC does not synchronize with PHY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8349 TSEC does not synchronize with PHY

1,278 Views
EAlepins
Contributor V

Hi,

We are using an Inphi LXT971A PHY connected to the TSEC1 of our MPC8349. We have followed the initialization steps recommendations in the MPC8349 RM. However, sometimes, the Ethernet driver initialization hangs when waiting for MACCFG1[Sync’d Rx EN] and [Sync’d Tx EN] to be set after we have set MACCFG1[Rx_EN and Tx_EN]. Both bits stay zero. We don't understand why. This is hard to reproduce. When it happens, we restart the whole Ethernet driver initialization and then it often works.

But still, we don't understand the meaning of these bits. What is "synchronization"? I am guessing that it is the PHY that is not doing something properly. But what? Knowing that could point us where to look in the PHY registers to see why it hangs.

Is "Sync’d Tx EN" an image of a certain external signal between TSEC and PHY? I don't see any one matching this in RM §15.4 "External Signals Description".

We work in MII. Our ECNTRL is 0x00001000. And MACCFG2 = 0x00007107.

Thanks.

Étienne

Labels (1)
0 Kudos
Reply
1 Reply

1,179 Views
ufedor
NXP Employee
NXP Employee

MACCFGC1[Sync'd Rx EN] and MACCFGC1[Sync'd Tx EN] reflect the status of MACCFGC1[Rx_EN] and MACCFGC1[Tx_EN] in the Rx Clock and Tx Clock domains, respectively. For example, a write to MACCFGC1[Rx_EN] is done in an internal HCLK domain.

Setting this bit does not affect the MAC until its value is translated in the RX_CLK domain.
When MACCFGC1[Rx_EN] is translated from the HCLK domain to the RX_CLK domain, MACCFG1[Sync'ed RxEN] changes. When MACCFG1[Sync'ed RxEN] is set, the MAC is enabled for Receiving on the Ethernet interface. Same holds true for transmitting.

Assuming that TX_CLK and RX_CLK are provided by PHY it is needed to check the PHY strapping/initialization.

0 Kudos
Reply