Flash Programming error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Programming error

4,245 Views
samyukta_s
Contributor I

Hi,

 

I am working on a Board which has MPC8360 Power PC. I am not able to program the flash which is interfaced to the Power PC. When monitored the LWE (write enable) signal we are getting high, where as in other working boards its pulsing. May i know how to rectify this?

 

Thanks,

Samyukta

0 Kudos
Reply
9 Replies

4,131 Views
ufedor
NXP Employee
NXP Employee

1) Was the board checked for a manufacturing/soldering issue?

2) Is the flash chip-select pulsed?

3) Is the LWE probed directly on the processor's pin?

0 Kudos
Reply

4,132 Views
samyukta_s
Contributor I
Dear Sir,
1) Was the board checked for a manufacturing/soldering issue?
Yes, its checked.
2) Is the flash chip-select pulsed?
yes , its pulsing. We have replaced the board with new flash IC.
3) Is the LWE probed directly on the processor's pin?
The processor pin is interfaced with a resistor(33 ohm) to the flash. We probed at the resistor end.
0 Kudos
Reply

4,131 Views
ufedor
NXP Employee
NXP Employee

4) Please use a debugger, execute write operation to the Flash LBC memory bank (chip-select) and check the LWE0 behaviour.

0 Kudos
Reply

4,131 Views
samyukta_s
Contributor I

Dear Sir,

4) Please use a debugger, execute write operation to the Flash LBC memory bank (chip-select) and check the LWE0 behaviour.

We checked it LWE0 is always high, whereas in other working boards its pulsing.

Thanks & Regards,

Samyukta Sudheendra

E-1181

Systems Engineer

Communications (Radio Relay)

ALPHA DESIGN TECHNOLOGIES PVT LTD

No. 271, 6th Main, Defence Colony 100ft Road, Indira Nagar, Bangalore - 560 038, India

Tel: +91-80-4255 6506| Fax: +91-80-4255 6523| Mob: +91 9901782861| Email: [email protected]<mailto:[email protected]>

<mailto:[email protected]>

<mailto:[email protected]>

0 Kudos
Reply

4,131 Views
ufedor
NXP Employee
NXP Employee

Please use a debugger to ensure that settings of LBC registers are identical on operational and problem boards.

If the LBC settings are identical, please perform the ABA swap - i.e. interchange processors between operational and problem boards.

0 Kudos
Reply

4,131 Views
samyukta_s
Contributor I

Dear Sir,

The LBC registers are identical for operational and problem boards.

With Regards,

Samyukta

0 Kudos
Reply

4,131 Views
ufedor
NXP Employee
NXP Employee

Please perform the ABA swap - i.e. interchange processors between operational and problem boards.

0 Kudos
Reply

4,131 Views
samyukta_s
Contributor I

Dear Sir,

We have replaced the processor with new IC. Even after the replacement, there is no improvement.

Please guide.

With Regards,

Samyukta 

0 Kudos
Reply

4,131 Views
ufedor
NXP Employee
NXP Employee

Please check that RCW is supplied correctly and is the same as on operational boards.

You wrote:

> The processor pin is interfaced with a resistor(33 ohm) to the flash.

What are measured levels when the resistor is removed?

0 Kudos
Reply