MPC8347 BSDL file and bscan

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8347 BSDL file and bscan

ソリューションへジャンプ
2,571件の閲覧回数
Timothy1
Contributor I

Hello, 

I am working on a testing harness for a PCB using the MPC8347 processor. I have a cable programmer and matching software already, but I can not seem to get ahold of the BSDL for the MPC8347. 

Any help or suggestions is greatly appreciated. Feel free to ask for more info and if it will help. 

Thank you. 

0 件の賞賛
返信
1 解決策
2,556件の閲覧回数
ufedor
NXP Employee
NXP Employee

The model in question is confidential and can be provided if NDA is present.

To request the model please create a Technical Case using your corporate email:

https://support.nxp.com/s/

元の投稿で解決策を見る

2 返答(返信)
2,557件の閲覧回数
ufedor
NXP Employee
NXP Employee

The model in question is confidential and can be provided if NDA is present.

To request the model please create a Technical Case using your corporate email:

https://support.nxp.com/s/

2,540件の閲覧回数
Timothy1
Contributor I

Thank you for this information! 

0 件の賞賛
返信