MPC8347 BSDL file and bscan

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8347 BSDL file and bscan

Jump to solution
2,582 Views
Timothy1
Contributor I

Hello, 

I am working on a testing harness for a PCB using the MPC8347 processor. I have a cable programmer and matching software already, but I can not seem to get ahold of the BSDL for the MPC8347. 

Any help or suggestions is greatly appreciated. Feel free to ask for more info and if it will help. 

Thank you. 

0 Kudos
Reply
1 Solution
2,567 Views
ufedor
NXP Employee
NXP Employee

The model in question is confidential and can be provided if NDA is present.

To request the model please create a Technical Case using your corporate email:

https://support.nxp.com/s/

View solution in original post

2 Replies
2,568 Views
ufedor
NXP Employee
NXP Employee

The model in question is confidential and can be provided if NDA is present.

To request the model please create a Technical Case using your corporate email:

https://support.nxp.com/s/

2,551 Views
Timothy1
Contributor I

Thank you for this information! 

0 Kudos
Reply