MPC8313 NAND Flash Boot reset command

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8313 NAND Flash Boot reset command

2,056件の閲覧回数
Metalik
Contributor I

Hi,

In my design I'm using MPC8313 processor. I got a problem with NAND chip obsolescence so manufacturer gives me proposal of a new device. Unfortunately the new one got statement that "Reset command needs to be applied before any operation".

Does FCM sends such command (0xFF) to the NAND flash during boot, before reading Reset Configuration Word ?

0 件の賞賛
返信
1 返信

1,945件の閲覧回数
r8070z
NXP Employee
NXP Employee

Reset command (0xFF) is common NAND flash command. It should be first command after system reset. I am sure the MPC8313 FMC sends such command (0xFF) to the NAND flash before read NAND page with Reset Configuration Word.

0 件の賞賛
返信