PCIe reset for T1042

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe reset for T1042

2,455件の閲覧回数
utkarsh_100
Contributor I

Hi All 

I am referring QorIQ T1040 Reference Manual  for my board T1042 where I want to reset the only pcie . But I could not able to find out how to reset the pcie .

Then I referred QorIQ T1040 Reference Design Board User Guide where I found out CPLD under that RSTCON2 register from which I can reset the PCIe 

After memory mapping for the for RSTCON2 register on my vxworks platform I tried to write 1 to clear for resetting the PCIe , but not sure whether it got reset or not . 

When I read default value RSTCON2 it was 0xFF ,but after writing also on pcie bit  its still 0xFF . (no change)

I have few question related to my comments 

1. How can I know CPLD is present on my target board T1042 since in refernce manual I could not find out anything related to that. 

2.Is there any other way I can reset only pcie interface . 

Thanks in advance  

0 件の賞賛
返信
2 返答(返信)

2,316件の閲覧回数
Bulat
NXP Employee
NXP Employee

You seem to mix up different reset terms. The only way to reset PCI Express interface of the processor is to reset the processor using PORESET or HRESET.

T1040 Reference Design Board (T1040RDB, T1042RDB) contains three PCIe connectors, two Mini PCIe and one PCIe x1 slot. The board has a feature allowing to assert reset signals going to each of these connectors, this is realised via on-board CPLD. RSTCON2 register located in the CPLD controls those reset signals, so the user is able to assert reset individually for each slot in software. You have to understand that the CPLD is an external device to the T1040/T1042, not the part of the processor. That is why it is not described in the QorIQ T1040 Reference Manual.

Regards,

Bulat

0 件の賞賛
返信

2,316件の閲覧回数
shaneggpierce
Contributor I

utkarsh_100 wrote:

Hi All 

I am referring QorIQ T1040 Reference Manual  for my board T1042 where I want to reset the only pcie . But I could not able to find out how to reset the pcie .

Then I referred QorIQ T1040 Reference Design Board User Guide where I found out CPLD under that RSTCON2 register from which I can reset the PCIe 

After memory mapping for the for RSTCON2 freejobalert gimp notepad++ register on my vxworks platform I tried to write 1 to clear for resetting the PCIe , but not sure whether it got reset or not . 

When I read default value RSTCON2 it was 0xFF ,but after writing also on pcie bit  its still 0xFF . (no change)

 

I have few question related to my comments 

 

1. How can I know CPLD is present on my target board T1042 since in refernce manual I could not find out anything related to that. 

 

2.Is there any other way I can reset only pcie interface . 

 

Thanks in advance  

I also have similar questions. Help is appreciated.


Thanks in advance.
Regards

Shane

0 件の賞賛
返信