MPC8309 tower Boot from SPI EEPROM Device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8309 tower Boot from SPI EEPROM Device

2,343 Views
ganjiaravind
Contributor I

Hi :

I am trying to Boot my freescale mpc8309 tower Board through SPI eeprom device ,can anyone here to guide me with your best suggestion ??Thank you in advance.

0 Kudos
Reply
1 Reply

2,014 Views
Pavel
NXP Employee
NXP Employee

Look at the AN3659 for SPI boot:

https://www.nxp.com/docs/en/application-note/AN3659.pdf?fsrch=1&sr=1&pageNum=1

 

Look at also attached file. This file is available in LTIB Linux BSP for the MPC8309SOM:

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=MPC8309-KIT_Linux_BSP


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply