I'm involved in designing fast charging and battery management system with cell balancing for Li-ion Battery

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I'm involved in designing fast charging and battery management system with cell balancing for Li-ion Battery

1,058 Views
sivanatrajan
Contributor I

Like to know,if there is single IC with fast charging,cell balancing capability.

How to combine NXP Fast charging IC and cell balancing IC for same battery pack.

IC suggestion for fast charging and cell balancing are welcomed

Battery details

Cell voltage :3.3V

Cell AH : 26AH

no.of battery :3

Connection : Series

0 Kudos
Reply
1 Reply

929 Views
Pavel
NXP Employee
NXP Employee

Look at the following page:

Battery Management|NXP 


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply