yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Ajay Bhargav,
It is possible, please try the following method.
On MPC8309SOM, the NOR Flash is allocated as the following.
Range Start Range End Definition
0xfe00_0000 0xfe05_ffff U-Boot
0xfe0a_0000 0xfe2f_ffff Kernel
0xfe30_0000 0xfe7e_ffff Ramdisk file system
0xfe7f_0000 0xfe7f_3fff DTB
Under u-boot after deploying uImage, rootfs.ext2.gz.uboot and dtb file at the specific addresses, and configure u-boot environment as the following.
setenv ramargs 'setenv bootargs root=/dev/ram rw console=ttyS0,115200'
setenv bootcmd 'run ramargs; bootm 0xfe0a0000 0xfe300000 0xfe7f0000'
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yiping,
even if I run uImage from NOR (which I am doing already), U-Boot relocates kernel to RAM before running it from Flash.
Display message "Loading Kernel Image... OK"
and after that dtb gets relocated to ram at a different address and then booting starts.
So "Loading Kernel Image... OK" itself takes around ~1sec. which I want to eliminate here. Any suggestions?
Regards,
Ajay Bhargav
 
					
				
		
 scottwood
		
			scottwood
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		This is not normally supported by U-Boot with bootm, though you might be able to do it without U-Boot changes by using the bootm subcommands and skipping loados, with the uImage specifying the flash address as the entry point.
However, that isn't going to make Linux run out of flash -- it just means that early Linux code will do the copy instead.
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Ajay Bhargav,
Would you please attach the whole Kernel boot log?
Thanks,
Yiping
Here is the u-boot + kernel log.
My kernel and u-boot is ported from stock MPC8309 kernel v2.6.34 that comes with Ltib. I am testing it on MPC8309 KIT.
U-Boot 2014.04-g678d3b1 (Dec 17 2014 - 17:12:45)MPC83XX
Reset Status:
CPU: e300c3, MPC8309E, Rev: 1.1 at 333.333 MHz, CSB: 133.333 MHz
Board: MPC8309 Test Board
Watchdog enabled
I2C: ready
DRAM: 256 MiB (DDR2, 32-bit, ECC off, 266.667 MHz)
Flash: 32 MiB
Firmware 'Microcode version 0.0.0 for MPC8306 r1.0' for 8306 V1.0
QE: uploading microcode 'Microcode for MPC8306 r1.0'
NAND: 512 MiB
MMC: FSL_SDHC: 0
In: serial
Out: serial
Err: serial
Net: UEC0, UEC1
Hit any key to stop autoboot: 0
MPC8309> mtdparts
device nor0 <nor>, # parts = 7
#: name size offset mask_flags
0: UBoot 0x00100000 0x00000000 0
1: env 0x00020000 0x00100000 0
2: ucode 0x00020000 0x00120000 0
3: dtb 0x00020000 0x00140000 0
4: reserved 0x000a0000 0x00160000 0
5: kernel 0x00800000 0x00200000 0
6: fs 0x01600000 0x00a00000 0
device nand0 <nand>, # parts = 4
#: name size offset mask_flags
0: UBoot-nand 0x00180000 0x00000000 0
1: DTB-nand 0x00080000 0x00180000 0
2: Kernel-nand 0x00800000 0x00200000 0
3: fs-nand 0x1f600000 0x00a00000 0
active partition: nor0,0 - (UBoot) 0x00100000 @ 0x00000000
defaults:
mtdids : nor0=nor,nand0=nand
mtdparts: mtdparts=nor:1M(UBoot),128K(env),128K(ucode),128K(dtb),640K(reserved),8M(kernel),-(fs);nand:1536K(UBoot-nand),512K(DTB-nand),8M(Kernel-nand))
MPC8309> boot
## Booting kernel from Legacy Image at fe200000 ...
Image Name: MPC8309 Linux 2.6.39
Image Type: PowerPC Linux Kernel Image (uncompressed)
Data Size: 4133632 Bytes = 3.9 MiB
Load Address: 00000000
Entry Point: 00000000
## Flattened Device Tree blob at fe140000
Booting using the fdt blob at 0xfe140000
Loading Kernel Image ... OK
Loading Device Tree to 007fa000, end 007ff46b ... OK
setup_arch: bootmem
mpc8309_setup_arch()
arch: exit
rtc-m41t80 0-0068: hctosys: unable to read the hardware clock
Creating mount points
Starting logging: OK
Initializing random number generator... done.
Starting network...
sd 0:0:0:0: [sda] Assuming drive cache: write through
sd 0:0:0:0: [sda] Assuming drive cache: write through
sd 0:0:0:0: [sda] Assuming drive cache: write through
udhcpc (v1.22.1) started
Sending discover...
Sending discover...
Sending discover...
No lease, failing
udhcpc (v1.22.1) started
Sending discover...
Sending discover...
Sending discover...
No lease, failing
Starting dropbear sshd: OK
Mounting USB Storage Device: OK
Welcome to Buildroot
mpc8309 login:
My Bootargs and bootcommand is:
bootargs=console=ttyS0,115200n8 root=ubi0:rootfs rw ubi.mtd=10,2048 noinitrd rootfstype=ubifs rootwait quiet
bootcmd=bootm 0xfe200000 - 0xfe140000
As you can see both kernel and dtb gets relocated before booting:
Loading Kernel Image ... OK
Loading Device Tree to 007fa000, end 007ff46b ... OK
Thanks in advance.