MPC8309 get precise time from rtc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8309 get precise time from rtc

ソリューションへジャンプ
2,799件の閲覧回数
威杨
Contributor III

Dear All,

               I am new to the MPC world and facing a problem,.i want to get a precise time from the rtc,time accuracy is 1 ms,but the rtc is 1s , i refer to the kernel module ieee 1588 source code,from it can get 1ms,but i can‘t use it sepreate the module.can you support some examples that can tell how to use the  rtc ?

Thanks & Regards

yang

ラベル(1)
0 件の賞賛
返信
1 解決策
2,510件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The accuracy of the RTC depends on its clock source. The RTC block is just timer which counts clock cycles from the clock source.

The IEEE 1588 protocol is used to synchronize the clocks of two systems, hardware provide time stamping but software compare time stamps, you could refer to http://cache.freescale.com/files/32bit/doc/app_note/AN3423.pdf .

For your purpose, probably you could refer to arch/powerpc/kernel/time.c, regarding generating precise time in Linux Kernel. If you only want to generate 1ms count, you also could use Timer.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,511件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The accuracy of the RTC depends on its clock source. The RTC block is just timer which counts clock cycles from the clock source.

The IEEE 1588 protocol is used to synchronize the clocks of two systems, hardware provide time stamping but software compare time stamps, you could refer to http://cache.freescale.com/files/32bit/doc/app_note/AN3423.pdf .

For your purpose, probably you could refer to arch/powerpc/kernel/time.c, regarding generating precise time in Linux Kernel. If you only want to generate 1ms count, you also could use Timer.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信