On MPC7448 system exception

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

On MPC7448 system exception

1,590件の閲覧回数
stefanodigiulio
Contributor I

On MPC7448 Is possible via system exception capture, get the below informations.

-Processor.overload

- Arithmetic overflow

- Illegal program instruction

- Memory corruption

regards

Stefano

0 件の賞賛
返信
1 返信

1,506件の閲覧回数
LPP
NXP Employee
NXP Employee

In the standalone system environment, the user software is responsible for handling the exceptions. Provide handlers for each exception involved in order to process or monitor. MPCFPE32B chapter 6 describes the context for all exceptions.

http://www.freescale.com/files/product/doc/MPCFPE32B.pdf

Now, about the cases:

- Processor.overload

what do you mean? 7448 has no "overload" state. Processor executes instruction stream continuously unless it is in sleep state. You might think about "overload" as if the processor is not able to meet the application performance requirments (e.g. can't process video on fly). This case should be managed by the application.

- Arithmetic overflow

Power Architecture instructions do not assert exceptions on the arithmetic overflows but report the overflow status in the XER register so that software can further handle this conditions properly. It can be done easily in assembler but not in high level language. Typical "C" compiler does does not check for arithmetic overflow.

http://www.fefe.de/intof.html

Floating point exceptions can be handled in software. Please refer to the fenv.h description in "MSL C Reference.pdf".

- Illegal program instruction

Program exception 0x00700 is raised on illegal instruction. The registers involved are SRR0,SRR1,MSR. Please refer to Section 6.5.7 of MPCFPE32B.

- Memory corruption

7448 implements the machine check exception 0x200 to handle system bus errors like L1/L2 cache errors. External memory controller (TSI108/109) which support ECC may provide error signaling to the same exception vector. 


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信