MPC8309 Vxworks BSP support.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8309 Vxworks BSP support.

1,351 次查看
saravanakumar_s
Contributor I

Does Vxworks BSP supports MPC8309 Processor. If so do we have any limitation. Please confirm?

0 项奖励
回复
1 回复

1,139 次查看
lunminliang
NXP Employee
NXP Employee

Hello Saravana Kumar,

Please kindly see below link:

Freescale Connect - Partner Profile Information

In the row VXWORKS BSPs, click "Devices", and you'll the supported devices list, there is no MPC8309 in the list.

Also on Windriver website of BSP list for Freescale:

Locate by Vendor - Freescale, Inc. - Wind River Board Support Packages

In the "Processor Family" column, choose "Freescale MPC83xx", you'll find that there are WRL4.3 and 4.2 for MPC8306 MPC8309, no VxWorks for MPC8309.

For MPC8309, Freescale provide "Linux BSP for Freescale MPC8309-KIT" which is available from:

BSPs for Power Architecture|MPC83xx|Freescale


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复