MPC8309 Vxworks BSP support.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8309 Vxworks BSP support.

1,339 Views
saravanakumar_s
Contributor I

Does Vxworks BSP supports MPC8309 Processor. If so do we have any limitation. Please confirm?

0 Kudos
Reply
1 Reply

1,127 Views
lunminliang
NXP Employee
NXP Employee

Hello Saravana Kumar,

Please kindly see below link:

Freescale Connect - Partner Profile Information

In the row VXWORKS BSPs, click "Devices", and you'll the supported devices list, there is no MPC8309 in the list.

Also on Windriver website of BSP list for Freescale:

Locate by Vendor - Freescale, Inc. - Wind River Board Support Packages

In the "Processor Family" column, choose "Freescale MPC83xx", you'll find that there are WRL4.3 and 4.2 for MPC8306 MPC8309, no VxWorks for MPC8309.

For MPC8309, Freescale provide "Linux BSP for Freescale MPC8309-KIT" which is available from:

BSPs for Power Architecture|MPC83xx|Freescale


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply