MPC8309 PCI for Agent Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8309 PCI for Agent Mode

Jump to solution
1,209 Views
威杨
Contributor III

Dear everyone,

     I want to use MPC8309 as the pcislave in uboot,i see

pastedImage_0.png

but i dont know configure which register.please give me some advises.

Have A Good Day !

0 Kudos
Reply
1 Solution
1,077 Views
alexander_yakov
NXP Employee
NXP Employee

Vendor ID and device ID registers are described in Sections 23.3.3.1 and 23.3.3.1 of MPC8309 Reference Manual.

PIWARn registers - Section 23.3.2.14

PCI function configuration register - Section 23.3.3.24


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,078 Views
alexander_yakov
NXP Employee
NXP Employee

Vendor ID and device ID registers are described in Sections 23.3.3.1 and 23.3.3.1 of MPC8309 Reference Manual.

PIWARn registers - Section 23.3.2.14

PCI function configuration register - Section 23.3.3.24


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply