MPC8309 PCI for Agent Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8309 PCI for Agent Mode

ソリューションへジャンプ
1,113件の閲覧回数
威杨
Contributor III

Dear everyone,

     I want to use MPC8309 as the pcislave in uboot,i see

pastedImage_0.png

but i dont know configure which register.please give me some advises.

Have A Good Day !

0 件の賞賛
返信
1 解決策
981件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Vendor ID and device ID registers are described in Sections 23.3.3.1 and 23.3.3.1 of MPC8309 Reference Manual.

PIWARn registers - Section 23.3.2.14

PCI function configuration register - Section 23.3.3.24


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
982件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Vendor ID and device ID registers are described in Sections 23.3.3.1 and 23.3.3.1 of MPC8309 Reference Manual.

PIWARn registers - Section 23.3.2.14

PCI function configuration register - Section 23.3.3.24


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信