MPC8309 / NOR BOOT Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8309 / NOR BOOT Issue

1,689 Views
pavanvora
Contributor I

Hello,

We have used MPC8309 Power QUICC II Pro processor in our new design and we have the assembled prototype board ready with us.

In out initial testing we are struggling to get the UBOOT code running through NOR BOOT and we are not able to get any data on console.

Here, we are able to connect the processor core through JTAG and are able to read / write NOR flash connected on eLBC with 16-bit GPCM interface.

We are using M29W256GH70ZS6E NOR flash.

Please let us know what could be the problem here stopping the processor to get BOOT from NOR.

Also let us know if you need more information related to design.  

Regards,

Pavan

0 Kudos
Reply
1 Reply

1,508 Views
catalindemergia
Contributor IV

Hi,

The console messages are sent after the bootloader's relocation in RAM. It could be a problem

with the DDR initialization. You sad you can read/write in flash. How did you do it, did you use the Flash Programmer

utility in CW ? I'm asking because CW downloads the flash algorithm code in RAM, so the RAM is initialized by CW

according to the target init file.

What about the flash content ? did you build a Freescale SDK that supports 8309 and wrote it into flash ?

regards

Catalin

0 Kudos
Reply