MPC8308

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8308

3,404件の閲覧回数
venkateshn
Contributor II

Hi,

In MPC838 i have following clarifications,

1)  eTSEC IO Supply for RGMII will be 2.5V as per the datasheet but in reference design  LVDD1(NVDDF1) is connected to 2.5V and LVDD2(NVDDC1) is connected to 3.3V but i am thinking LVDD2 also needs to connect 2.5V so kindly clarify this.

2) for MPC8308 it is required to use VTT for DDR? in reference design they have not included this section and i am using only one device with 128MB density having organization 64MX16 so kindly clarify the VTT requirement.

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

3,104件の閲覧回数
Bulat
NXP Employee
NXP Employee

1) The MPC8308 is able to support RGMII with either 2.5V or 3.3V supply. You are right, normally RGMII works at 2.5V, however the PHY in the ref design requires 3.3V supply on the RGMII interface.  That is why eTSEC1 is powered with 3.3V to be on the same power rail with the PHY.

2) Yes, the ref design does not have VTT termination on the DDR interface. You can use this experience in your design, especially if you have point-to-point connections on the address/command/control signals.

Regards,

Bulat

0 件の賞賛
返信

3,104件の閲覧回数
venkateshn
Contributor II

Hi

0 件の賞賛
返信