MPC8245 datasheet : absolute max rating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8245 datasheet : absolute max rating

1,485件の閲覧回数
stephanelaffont
Contributor IV

Hello, could you confirm the temperature absolute max rating specified in the MPC8245 datasheet ?

The value is currently 105°C, the same a the recommended value. Usually there is some margin between those 2 values.

Thanks for your help.

Best regards,

Stéphane

タグ(1)
0 件の賞賛
返信
1 返信

1,313件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes, operational die-junction temperature range in the Absolute Maximum Ratings and Die-junction temperature in the Recommended Operating Conditions are the same.

Notice that for the next power processor generations like MPC83xx, MPC85xx they provide only Storage temperature range in the Absolute Maximum Ratings, while the maximal die junction temperature limits the Recommended Operating Condition.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信