MPC8245 datasheet : absolute max rating

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8245 datasheet : absolute max rating

1,474 Views
stephanelaffont
Contributor IV

Hello, could you confirm the temperature absolute max rating specified in the MPC8245 datasheet ?

The value is currently 105°C, the same a the recommended value. Usually there is some margin between those 2 values.

Thanks for your help.

Best regards,

Stéphane

Tags (1)
0 Kudos
Reply
1 Reply

1,302 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes, operational die-junction temperature range in the Absolute Maximum Ratings and Die-junction temperature in the Recommended Operating Conditions are the same.

Notice that for the next power processor generations like MPC83xx, MPC85xx they provide only Storage temperature range in the Absolute Maximum Ratings, while the maximal die junction temperature limits the Recommended Operating Condition.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply