LS1046A DDR4 interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A DDR4 interface

Jump to solution
2,295 Views
Nareshvarikuntla
Contributor III

Dear NXP,

Can I interface just 32 bit DDR4 with ECC memory to LS1046A. Could please provide references in this regard.

Regards,

Naresh V.

0 Kudos
Reply
1 Solution
2,284 Views
ufedor
NXP Employee
NXP Employee

> Can I interface just 32 bit DDR4 with ECC memory to LS1046A.

Yes.

> Could please provide references in this regard.

Please refer to the FRWY-LS1046A schematics available at:

https://www.nxp.com/design/qoriq-developer-resources/ls1046a-freeway-board:FRWY-LS1046A?fpsp=1#Desig...

For 32-bit case do not implement U17 and U18.

Assuming that Accumulated ECC will be enabled, D1_MECC[4-7] have to be left unconnected.

View solution in original post

0 Kudos
Reply
1 Reply
2,285 Views
ufedor
NXP Employee
NXP Employee

> Can I interface just 32 bit DDR4 with ECC memory to LS1046A.

Yes.

> Could please provide references in this regard.

Please refer to the FRWY-LS1046A schematics available at:

https://www.nxp.com/design/qoriq-developer-resources/ls1046a-freeway-board:FRWY-LS1046A?fpsp=1#Desig...

For 32-bit case do not implement U17 and U18.

Assuming that Accumulated ECC will be enabled, D1_MECC[4-7] have to be left unconnected.

0 Kudos
Reply