LS1046A DDR4 interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A DDR4 interface

ソリューションへジャンプ
2,310件の閲覧回数
Nareshvarikuntla
Contributor III

Dear NXP,

Can I interface just 32 bit DDR4 with ECC memory to LS1046A. Could please provide references in this regard.

Regards,

Naresh V.

0 件の賞賛
返信
1 解決策
2,299件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Can I interface just 32 bit DDR4 with ECC memory to LS1046A.

Yes.

> Could please provide references in this regard.

Please refer to the FRWY-LS1046A schematics available at:

https://www.nxp.com/design/qoriq-developer-resources/ls1046a-freeway-board:FRWY-LS1046A?fpsp=1#Desig...

For 32-bit case do not implement U17 and U18.

Assuming that Accumulated ECC will be enabled, D1_MECC[4-7] have to be left unconnected.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,300件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Can I interface just 32 bit DDR4 with ECC memory to LS1046A.

Yes.

> Could please provide references in this regard.

Please refer to the FRWY-LS1046A schematics available at:

https://www.nxp.com/design/qoriq-developer-resources/ls1046a-freeway-board:FRWY-LS1046A?fpsp=1#Desig...

For 32-bit case do not implement U17 and U18.

Assuming that Accumulated ECC will be enabled, D1_MECC[4-7] have to be left unconnected.

0 件の賞賛
返信