LS1012AXE7HKA SPI interface frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012AXE7HKA SPI interface frequency

1,199 Views
manojkumar_kaki
Contributor I

Kindly provide us the SPI frequency of operation modes supported by LS1012 MCU.

Thanks

manoj.

0 Kudos
Reply
1 Reply

1,116 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

LS1012A SPI clock frequency depends on platform frequency, SPI_CTARn[DBR], SPI_CTARn[PBR] and SPI_CTARn[BR]. SPI clock frequency = platform frequency *((1 + DBR )/(Prescaler * Scaler)). So we can set SPI frequency up to 125MHz*(1+1)/(2*2) = 62.5MHz. Next we have to take into account SPI AC timing specifications for LS1012A and connected SPI slave. For details please see “Calculating the maximum SPI frequency” in the nxp application note
https://www.nxp.com/docs/en/application-note/AN4375.pdf

The LS1012A SPI AC timing specifications you can find in the LS1012A datasheet available on the nxp site.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply