Issues in SPI Boot on custom T2081

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues in SPI Boot on custom T2081

1,278件の閲覧回数
Irfan3
Contributor III

Hi Team,

We are working on SPI NOR boot in T2081 custom board.
 
We were able to load the U-boot into the SPI NOR device and it was running till DDR Initialization failed.
 
While DDR debug due to DDR init fail, with some changes in hardware, now we are not able to boot-up at all.
 
We have cross checked the dump of the flashed file with the input file and it's same. Also, we have checked the loaded file and configuration of PBL from software side, it's not changed at all.
 
Could you please suggest us how to debug this issue.
 
Thanks and Regards,
Irfan
0 件の賞賛
返信
1 返信

1,268件の閲覧回数
ufedor
NXP Employee
NXP Employee

> While DDR debug due to DDR init fail, with some changes in hardware

Which exactly hardware changes?

0 件の賞賛
返信